To Clear the Gemini RAM memory (all configuration and working data will be lost)

1. First set the PC serial COM port configuration for 57600baud, 8 bits, no parity, no handshake using a terminal program such as Hyperterm.

2. Connect the PC serial port to the Gemini handset port.

3. Press the small reset button near the front edge of the Gemini processor card and as soon as the reset button is released, enter <Ctrl-C> on the PC terminal a number of times i.e. hold down the Ctrl key and then press the C key a number of times.

4. If the RedBoot prompt does not appear, reset and try again. Also check that the serial port settings are correct and that the serial cable is "straight through" and not a null modem or cross-over. If no response can be obtained from the unit then it will need to be returned to Poole for repair.

5. Clear the Gemini RAM memory, enter the command

mfill -b 0x14000 -l 0x100000 -p 0x0

6. Reset the Gemini unit and return the the PC serial COM port configuration to its normal Gemini setting 57600 or 19200baud, 7 bits, even parity. This time after reset, the Gemini unit should perform a first time startup and any configuration data, including facility licence codes will need to be re-entered.

To restore Redboot Version 2 startup script

If the unit enters Redboot following reset but does not run the Gemini application, then the startup script which is held at the end of the flash memory may have become corrupt. The following procedure will reprogram the startup script. The procedure is only required for Gemini units running Redboot V2.

1. First set the PC serial COM port configuration for 57600baud, 8 bits, no parity.

2. Enter the following commands in bold :-

RedBoot> fconfig

Run script at boot: true

Boot script:

Enter script, terminate with empty line

>> go 0x40020100

>>

Boot script timeout (1000ms resolution): 1

Update RedBoot non-volatile configuration - continue (y/n)? y

... Erase from 0x401c0000-0x401c1000: .

... Program from 0x001de000-0x001df000 at 0x401c0000: .

3. Then reset the unit by pressing the reset button on the CPU card.

Note that this only applies to Gemini units running Redboot V2. New Gemini units running Redboot version 4 or later do not have a configurable startup script.

How to check the version of RedBoot

Use the RIC command when running the application software e.g.:-

RIC

RIC:Redboot V2

Or in Redboot, type in the "vers" command:-

RedBoot> vers

RedBoot(tm) bootstrap and debug environment [ROM]

Non-certified release, version 2 - built 11:24:10, Jun 4 2003

Platform: SIEMENS PLUTO (PowerPC MPC850)

Copyright (C) 2000, 2001, 2002, Red Hat, Inc.

Compatibility ID: 0x0

RAM: 0x00000000-0x00200000, 0x000087f0-0x001dd000 available

FLASH: 0x40000000 - 0x40200000, 16 blocks of 0x00020000 bytes each.

RedBoot>

To Upgrade from Redboot Version 2 to Version 5

Moving from PB683 to PB684 will generate a flash checksum error on Redboot V2. The following procedure is required in order to load Redboot V5.

1. Use the upgrade tool to load PB684 Issue 6. (DO NOT load issues higher than 6 of PB684, as they do not contain Redboot V5 and will result in the Gemini1 unit becoming unresponsive and having to be returned to Siemens for repair)

2. Set the PC serial COM port configuration for 57600baud, 8 bits, no parity.

3. Press the small reset button near the front edge of the Gemini processor card and as soon as the reset button is released, enter <Ctrl-C> on the PC terminal a number of times i.e. hold down the Ctrl key and then press the C key a number of times.

4. If the RedBoot prompt does not appear, reset and try again. Also check that the serial port settings are correct and that the serial cable is "straight through" and not a null modem or cross-over.

5. Enter the Redboot command:

go 0x40020100

6. Change the PC serial COM port configuration to 57600baud, 7 bits, even parity.

7. Enter until the prompt appears. Enter the PIC command and check that "PIC:12684 ISS6" is displayed.

8. Enter the following Gemini commands:

PME=249

UPG=REDBOOT

9. The unit should program Redboot into flash and then restart.

10. Enter until the prompt appears, then use the RIC command to check the new Redboot version.